EGEAR.ACCLIMIT
Description
EGEAR.ACCLIMIT sets the maximum acceleration that will be commanded on the follower when EGEAR.ON is turned ON or the electronic gearing ratio (EGEAR.RATIO or EGEAR.PUSLESOUT / EGEAR.PUSLESIN ) is increased. This maximum acceleration limit remains in effect until EGEAR.LOCK is achieved. Once EGEAR.LOCK is achieved the follower will follow the master with whatever acceleration or deceleration is required.
EGEAR.ACCLIMIT is independent of EGEAR.DECLIMIT. Each variable must be set, independently, to the appropriate value for the desired motion.
Example
' This example shows how to use EGEAR.ACCLIMIT to limit ' acceleration and then make up the lost distance. EGEAR.ACCLIMIT = 10000 EGEAR.RATIO = 1 DRV.SWENABLE = 1 EGEAR.ERROR = 0 EGEAR.TYPE = 0 EGEAR.ON = 1 While EGEAR.LOCK = 0 : wend 'wait for LOCK MOVE.RELATIVEDIST = EGEAR.ERROR MOVE.GOREL
General Information
|
Type |
R/W |
|
Units |
Depends on UNIT.ACCROTARY or UNIT.ACCLINEAR Rotary: rps/s, rpm/s, deg/s², (Benutzerspezifische Einheiten)/s² , rad/s² Linear: counts/s² , mm/s² , µm/s² , (Benutzerspezifische Einheiten)/s² |
|
Range |
Note: The range and default values of (Benutzerspezifische Einheiten)/s² units depend on the values of PIN and POUT. The range and default values listed in this table are derived from the default values of PIN and POUT. Rotary: 0.004 to 8,000,000 rps/s 0.224 to 480,000,016.384 rpm/s 1.341 to 2,879,999,967.232 deg/s² 0.019 to 40,000,000 (Benutzerspezifische Einheiten)/s² 0.023 to 50,265,481.216 rad/s² Linear: 16,000,000 to 15,912,994,294,290,448.384 counts/s² 0.119*MOTOR.PITCH to 256,000,000*MOTOR.PITCH mm/s² 119.209*MOTOR.PITCH to 255,999,998,951.424*MOTOR.PITCH µm/s² 0.019 to 40,000,000(Benutzerspezifische Einheiten)/s² |
|
Default Value |
Note: The range and default values of (Benutzerspezifische Einheiten)/s² units depend on the values of PIN and POUT. The range and default values listed in this table are derived from the default values of PIN and POUT. Rotary: 166.669 rps/s 10,000.170 rpm/s 60,001.016 deg/s² 833.347 (Benutzerspezifische Einheiten)/s² 1,047.215 rad/s² Linear: 715,839,984,631.808 counts/s² 5,333.424*MOTOR.PITCH mm/s² 5,333,423.616*MOTOR.PITCH µm/s² 833.347 (Benutzerspezifische Einheiten)/s² |
|
Data Type |
Integer |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
|---|---|---|---|---|
|
Modbus |
1060 |
Yes | low 32 bit word | No |